Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

should I specify vector address for Interrupt/Exception Handlers?

Latest Updated:12/01/2011

Question:

I would like to ask a question about the description in 4.8 Describing "Interrupt/Exception Handlers" (p.77) of the CA850 C Compiler Package C Language User's Manual.
Can I register a function name pointer in the interrupt vector area by describing as instructed on p.78 [To specify the interrupt function].
Or should I define a specific vector address?
Can I describe an interrupt handler in C language only?

Answer:

You can describe an interrupt handler in C language only.
Suitable Products