Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Why is the following error message is output?

Latest Updated:12/01/2011

Question:

Why is the following error message is output?

Answer:

This error message is output when the branch enabled range (22 bits) of the jarl instruction used for function call in the CA850 is exceeded.
Specify the -Xfar_jump option.
For details, refer to 5.4 "Far jump Call from C Language Program" in the CA850 C Language User's Manual.
Suitable Products