Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What to do if InstallShield error 6001 is show during setup of IO Wizard?

Latest Updated:09/04/2009

Question:

What should user do if InstallShield error code - 6001 is encountered during setup of IO Wizard?

Answer:

This InstallShield error indicates a corrupt version of InstallShield is installed on your computer. To correct this issue, simply delete the following folder from your computer and attempt to run the installer again: C:\Program Files\Common Files\InstallShield\Professional\RunTime\0701

If this fails to correct the problem, we recommend you RENAME (not delete) the entire C:\Program Files\Common Files\InstallShield\ folder and try again.

You may rename the folder to anything you like, but we recommend something similar to 'InstallShield-old'.

Suitable Products