Pular para o conteúdo principal
Renesas Brasil - Knowledgebase

What error occurs during linking when build is executed?

Latest Updated:12/01/2011


The following error occurs during linking when build is executed.

*** ERROR A402 File 'xxxxxx.REL' has no string table for symbol Program Aborted.


This error indicates that the symbol table has been destroyed.
There are several possible causes, but first check the following points.

(1) If using an inline assembler in C, check local symbols that start with something other than ?L are defined.
(2) Check the length of function names that exceed 24 characters.
If there are such descriptions, change the symbol name.

Suitable Products