Pular para o conteúdo principal
Renesas Brasil - Knowledgebase

What's the difference between E-78K4-NS- IE-784000-R?

Latest Updated:12/01/2011


The following two in-circuit emulators seem to be available, but how do they differ.
- IE-78K4-NS
- IE-784000-R


The IE-78K4-NS is a new compact product, while the IE-784000-R is an old-type product.
In terms of functions, they are almost the same.
For new applications, we recommend the low-cost IE-78K4-NS.

(Supplementary information)
Only the IE-78K4-NS can be used for notebook PCs.
(I/F cards support only the IE-78K4-NS.)
Suitable Products
78K Family