Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Which factors may lead to an erasure error in libraries for RL78 MCUs?

Latest Updated:04/04/2014

Question:

Which factors may lead to an erasure error when running the following libraries for the RL78 family of MCUs?

  • Flash Self Programming Library Type01
  • Data Flash Library Type04

Answer:

Erasure taking an extremely long time due to a device having aged deterioration or not being processed correctly due to interruption of the power supply, or to noise leading to the power voltage being unstable, can be considered as possible factors.
Suitable Products
Flash Self Programming Libraries
Data Flash Libraries