Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What settings are needed for processing in the flash area?

Latest Updated:11/21/2014

Question:

In the sample program described in the RL78/G13 Flash Self Programming: Execution application note, what settings are needed to call processing in the flash area from boot_main processing in the boot area?

Answer:

The file r_fsl_praxis01_BranchTable.h of the sample program includes an example of the use of the #pragma ext_func to make the setting required for calling a function in the flash area from the boot area.

For details, refer to section 2.5, Configuring Projects (Relink Function Configuration), in the RL78/G13 Flash Self Programming: Execution application note, from here.

For details on '#pragma ext_func', refer to CubeSuite+ V2.00.00 Integrated Development Environment User's Manual: RL78, 78K0R Build, from here.

Suitable Products
Flash Self Programming Libraries