Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is it okay to define symbols like compiler for parameters in assembly?

Latest Updated:12/01/2011

Question:

Is it possible to define symbols in the same manner as with the compiler for parameters during assembly?

Answer:

This has become possible from RA78K0 V3.50.
Specification similar to the compiler using option -d is possible.
Perform specification as follows from the command line.

  C> ra78k0 k0main.asm c054 -dSYM
Or,
  C> ra78k0 k0main.asm c054 -dSYM=1

When performing specification with the Project Manager, input -dSYM or -dSYM=1 to "Other Options" on the "Other" page for the assembler option.

Suitable Products