Pular para o conteúdo principal
Renesas Brasil - Knowledgebase

Is it OK to upload hexadecimal data in ROM writer to PC and generate data?

Latest Updated:09/15/2006


I want to upload the hexadecimal data from the ROM writer to my PC and then generate mask data from the hexadecimal data by using MM. Is it possible?


A hexadecimal data file to be processed by MM must be directly generated by the development system. The hexadecimal data uploaded to your PC from the ROM programmer may include unnecessary data.
You will not be able to correctly generate mask data using such a file.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering