Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is a mask file different from an ordinary hexadecimal data file?

Latest Updated:09/15/2006

Question:

Is a mask file different from an ordinary hexadecimal data file?

Answer:

A mask file is of a file format that registers information specifically for masking Renesas microcomputers.
It is similar to a Motorola S format file, but it cannot be downloaded and used on a debugger. Also, do not edit it with an editor.
Editing will alter the mask file content and will prevent the microcomputer from being masked correctly.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering