Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

IE-78K4-NS, is EV-9200GF-100 correct for the uPD784216AGF?

Latest Updated:12/01/2011

Question:

In the IE-78K4-NS, is the EV-9200GF-100 the correct conversion socket for the uPD784216AGF?

Answer:

Yes, please use the EV-9200GF-100 as the conversion socket for a GF-type package.
Suitable Products