Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How to properly upgrade FDT V.3.07 Release 00 to V.3.07 Release 01?

Latest Updated:01/05/2007

Question:

[Flash Development Toolkit V.3] After upgrading from Flash Development Toolkit V.3.07 Release 00 to V.3.07 Release 01, I can not see if the upgrade has been completed properly from the program file.

Answer:

Because Flash Development Toolkit V.3.07 Release 00 and V.3.07 Release 01 share the same program file FDT.exe, it is not easy to check if it has been upgraded to V.3.07 Release01 properly. Follow the procedure below to see if it has been upgraded properly.
After upgrading Flash Development Toolkit, see the Readme file in the folder where Flash Development Toolkit is installed to check its version.
Suitable Products