Pular para o conteúdo principal
Renesas Brasil - Knowledgebase

How to properly set up the startup routine in compiler option?

Latest Updated:12/01/2011


I want to set the startup routine in the compiler option setting dialog box from the Project Manager, but the setting items are dimmed and cannot be set.


When any of the source files is selected in the left-side window of Project Manager (PM32 Project Window), the mode for setting individual source options is enabled, and as a result the startup routine cannot be set.
Please perform the compiler option settings after clicking a part other than the source file name in order to deselect the source file name, and then perform the compiler option settings.
Suitable Products