Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How to get the permanent key to the IAR Systems AB ICC740 for re issued?

Latest Updated:09/11/2006

Question:

I installed M3T-ICC740 V.1.00 Release 1B, and I need the IAR Systems AB ICC740 permanent key* to be re-issued.
(*The permanent key is still required even one month after installing IAR Systems Compiler ICC740 (bundled with M3T-ICC740 V.1.00 Release 1B).

Answer:

The ICC740 V.2.17A bundled with Compiler Package (M3T-ICC740) V.1.01 Release 00 (740 Family), which was upgraded in June 2005, no longer requires a permanent license key. In addition, the permanent key for all previous versions, V2.16A and older, is no longer available.

Please refer to the software revision for M3T-ICC740 V.1.01 Release 01 for more details.
From this version on, the compiler will operate in the High-performance Embedded Workshop integrated environment. Check RENESAS TOOL NEWS and M3T-ICC740 Release Notes for compatibility with older version and other usage notes.

Download the M3T-ICC740 V.1.01 Release 01 package here
Select the download title, “[740 Family C Compiler Package M3T-ICC740 V.1.01 Release 01 Update].

When downloading a file from the Renesas Electronics site for the first time, you will need to create an My Renesas account first. Please do so at this page.

Suitable Products