Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How to generate source codes from IO Wizard into HEW?

Latest Updated:09/04/2009

Question:

Why is it that I cannot export the generated source codes from IO Wizard into HEW?

Answer:

The prerequisite for the exporting to work is that HEW and HEW Target Server (COM) has already been installed on your machine. If HEW is already installed on your machine, please verify it is version 4.2 or above.

Suitable Products