Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How to build a program using the CA850 (Project Manager)?

Latest Updated:12/01/2011

Question:

I built a sample program using the CA850 (Project Manager).
When a _reset label is defined in the startup module, the following message is displayed. Why is this message displayed?
Is _reset a reserved word or is it defined in a library, etc.?

Answer:

_reset is not used in the CA850 but is used in the RX850.
We advise you not to use this symbol.
Suitable Products