Pular para o conteúdo principal
Renesas Brasil - Knowledgebase

Error Message: C3304 (F) Cannot delete internal file

Latest Updated:02/18/2013


The following compile error occurs in building.

C3304 (F) Cannot delete internal file


This error is output when an intermediate file created by the compiler cannot be deleted.
The following should be confirmed.

  • The error may be generated by the realtime search of an antivirus software.
    Temporarily disable the realtime search of the antivirus software during building.

  • Specify a location with a slow access speed (e.g., network drive) as the destination for setting SHC_TMP.

  • Execute a build using administrative authority.

Also refer to the FAQ below because the error might be prevented by the method described in the FAQ.
FAQ 106515

Suitable Products
C/C++ Compiler Package for SuperH Family