Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Do I have to specify the product name in the data area?

Latest Updated:09/15/2006

Question:

Do I have to specify the product name in the data area?

Answer:

When creating mask data with an older EPROM, the product name had to be set in ASCII code in the specified EPROM area.
However, with MM, mask name data is set in the mask file, therefore this data need not be set separately. Do not register product name data set by EPROM in the hexadecimal data file specified in the mask file.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering