Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Deselecting DP/Flash shield window for RL78 MCU using RFP/PG-FP5

Latest Updated:11/21/2014

Question:

How can I deselect the [Disable Program] and [Flash shield window] security settings for the flash memory of an RL78 MCU while using the following flash programmers?

  • Renesas Flash Programmer
  • PG-FP5

Answer:

To deselect the [Disable Program] and [Flash shield window] settings, you must first execute the Security Release command.
To execute the Security Release command, specify [Chip] as the [Operation Mode] of the flash programmer and press the [Erase] button.
Suitable Products
PG-FP5
Renesas Flash Programmer