Pular para o conteúdo principal
Renesas Brasil - Knowledgebase

Can this file name be set when building with the Project Manager?

Latest Updated:12/01/2011


When building with the Project Manager, load module (.lmf) file name becomes the first compiled file name.
Can this file name be set?


Yes, it is possible by setting a linker option.
In the Project Manager menu list, click "Option (O)", and the select "Linker Option Setting (L)" from the pull-down menu.
The screen then changes to the Option Setting Screen (Output 1), so set the file name that you want to set in the Output File Name field.
Suitable Products