Pular para o conteúdo principal
Renesas Brasil - Knowledgebase

Can I download the mask file to the debugger?

Latest Updated:09/15/2006


Can I download the mask file to the debugger?


The mask file is in the ROM mask-processing format. It cannot be used for debugging in a debugger or EPROM. To debug the hexadecimal data registered in the mask file, you will need to use a hexadecimal data file generated from an abstracted hexadecimal data file.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering