Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Can I create mask file from object file created using Intel HEX format?

Latest Updated:09/15/2006

Question:

Is it possible to create a mask file from an object file that was created using a partner assembler in Intel HEX format?

Answer:

MM can handle the following types of file formats.
1. Intel HEX format
2. Expanded Intel HEX format
3. Renesas Original HEX format
4. Motorola S1, S2 and S3 formats
Therefore, a mask file can be created as long as the assembler you are using can output in one of the above formats.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering