Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Are there requirements for using any of the RL78 family libraries?

Latest Updated:10/24/2014

Question:

What are the self-RAM area requirements if I use any of the following libraries for the RL78 family ?

  • Flash Self Programming Library Type01
  • Data Flash Library Type04
  • EEPROM Emulation Library Pack01
  • EEPROM Emulation Library Pack02

Answer:

The self-RAM area requirement for using a library depends on the RL78 MCU and library you are using. Download the list at the following link for details.

Suitable Products
Flash Self Programming Libraries
Data Flash Libraries