Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Are there recommended interval to execute EEL_Handler?

Latest Updated:04/23/2014

Question:

In the libraries for the RL78 below, is there any recommended interval for executing the EEL_Handler function while the EEL_Execute function is running?

  • EEPROM Emulation Library Pack01
  • EEPROM Emulation Library Pack02

Answer:

There is no recommended interval for executing the EEL_Handler function.
To suppress effects of the interval for calling the EEL_Handler function on the processing time of the EEL_Execute function, we recommend continuously executing the EEL_Handler function.
Suitable Products
Data Flash Libraries