Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Are there any point to use the libraries?

Latest Updated:12/01/2011

Question:

Are there any point to use the libraries?

Answer:

The point is what type of model (normal or static) is used and option.
For details, refer to the beginning of "Chapter 10 Library Functions" in the Manual (Language).
Suitable Products