Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

RI600V4 and RI600PX Sample Projects for FIT for RX651

Last Updated:02/21/2018

Question:

Do you provide RI600V4 and RI600PX sample projects for FIT for RX651?

Answer:

We can provide RI600V4 and RI600PX sample projects for FIT for RX65N, which can be used for RX651.
Since the only difference between RX65N and RX651 is whether EDMAC is included or not, the above sample projects are available for both RX65N and RX651.
However, since the sample projects are set for RX65N by default, to use them for RX651, you need to change the value of macro BSP_CFG_MCU_PART_GROUP from 0 to 1 by r_bsp_config.h.

Suitable Products

RI600V4
RI600PX
RX Family