Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How do I resolve the “C0530001: Internal Error” that appears while using the RL78 compiler CC-RL in combination with the RI78V4 V2 RTOS?

Latest Updated:05/17/2017

Question:

How do I resolve the “C0530001: Internal Error” that appears while using the RL78 compiler CC-RL in combination with the RI78V4 V2 RTOS?

Answer:

The error “C0530001” may occur when all the following conditions happen.

1.    Compile option “-g” has been specified.

2.    Compile option “-Opipeline” has been specified.
This option is available with V1.03.00 or later by default.

3.    “#pragma rtos_interrupt” or “#pragma rtos_task” has been specified.
With RI78V4 V2 these are automatically output to the file “kernel_id.h”.

The error can be resolved by either of the workarounds below.

1.    Not specify the compile option “-g”.
2.    Specify the compile option “-Opipeline=off”.
When using the IDE CS+, select “No” for "Pipeline optimization" in the "Compile Options" tabbed page on the Property panel of the CC-RL Build tool.

Note that the above two compile options can be specified for each source file. 

 

Suitable Products
RI78V4 V2 Real-time OS for RL78 Family
C Compiler Package for RL78 Family