Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Can I use the PIC or PID CC-RX with RI600V4 or RI600PX in operating system

Latest Updated:07/14/2015

Question:

Can I use the PIC or PID functions of CC-RX with the RI600V4 or RI600PX operating system?

Answer:

No, you cannot use the PIC and PID functions since they are not intended to be used with these operating systems. For this reason, PIC and PID options in the ritable.src file which is required by the RI600V4 or RI600PX are prohibited.
Suitable Products
RI600V4 Real-time OS for RX Family
RI600PX Real-time OS for RX Family