Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What is E8a emulator and the High-performance Embedded Workshop?

Latest Updated:02/08/2012

Question:

It is my first time to develop an application using the E8a emulator and the High-performance Embedded Workshop.
Can you tell me which documents will help me? Are there any information as references?

Answer:

Refer to the following.

  References Reference Sections Descriptions
Basic
Operations
E8a Emulator User's Manual Section 3 Preparation before Use through Section 6 Tutorial Installation of the High-performance Embedded Workshop through basic operations of the E8a emulator.
Renesas E8a On-Chip Debugging Emulator Introductory Guide for R8C Family Application Notes 4. Installing the Software through
6. Let's Try Using the E8a Emulator
For R8C Family MCUs users:
It provides simple descriptions regarding the E8a emulator to help the user easily follow a straight path from unpacking of the emulator to running and stopping a program without getting lost on the way.
Debugger
Functions
E8a Emulator User's Manual Section 2 E8a Emulator Functions The E8a emulator functions.
E8a Emulator Additional Document for User's Manual 6. E8a Emulator Functions (Supplement on the User’s Manual) The E8a emulator functions on specific MCUs.
High-performance Embedded Workshop User's Manual 17. Debugging Facility Common fuctions of emulator products operated under the High-performance Embedded Workshop.
[Emulator Help] in the High-performance Embedded Workshop [Help] menu - The E8a emulator functions +
The E8a emulator functions on specific MCUs.
[Help Topic] in the High-performance Embedded Workshop [Help] menu - Common fuctions of emulator products operated under the High-performance Embedded Workshop.
Troubleshootings E8a Emulator Additional Document for User's Manual 7. Notes on Using the E8a Emulator Restrictions of the E8a emulator on specific MCUs.
FAQs portal site for troubleshootings - FAQs portal site for troubleshootings on using the E8a emulator.
FAQs portal site for error messages - FAQs portal site for error messages outputted by the E8a emulator.
FAQ - FAQs for the E8a emulator.
Fault E8a Emulator User's Manual Appendix E E8aSCP (E8a Self-Check Program) The troubleshooting procedure that applies the self-check program for the E8a emulator (E8aSCP).
Latest
Information
Tool News - Information about the upgraded versions, the precautions and etc.
E8a Emulator Debugger Release Notes - Supported MCUs, Notes and Version Report
Etc. R8C Tiny Series E8a Emulator Application Note Write Facility of the Microcomputer's Internal Flash Memory - For R8C Family MCUs users:
The procedure for writing load module data into the flash memory after starting the E8a emulator in writer mode.
E8a Emulator Application Note Outline of the Start/Stop Feature and an Example of Its Application for Time Measurement - The outline of the Start/Stop feature and describes how to use the Start/Stop feature to measure the execution time of a user program as an example of its application.
FAQ portal site for E8a/E8 Know-How - FAQ portal site for E8a/E8 Know-How on using the E8a emulator.
Suitable Products
E8a