Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Warning message-Program size is exceeds Flash Memory size_E8a_E8

Last Updated:11/08/2017

Question:

When I downloaded a program in the Flash Memory Data Write-Only mode using E8a (or E8) for an H8 family MCU, the "program size is exceeds Flash memory size" warning appeared.

Answer:

This message indicates that some of the data of the downloaded program has been stored at an address located in an area other than MCU internal ROM. You will need to reference the map file to find the location of this data, and then make changes to the program or a section so that the data is assigned within the internal ROM area.

Suitable Products

H8 Family
E8
E8a