Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Resolution of Run Time Count function of E7 E8 or E8a emulator

Last Updated:10/18/2017

Question:

I measured the run time of my program using the Run Time Count function on the E7/E8/E8a emulators. However, the resolution of the timer is in milliseconds. Is it possible to get an even more precise measurement?

Answer:

The Run Time Count function on the E7/E8/E8a emulators uses the host PC as the timer resource. Therefore, a time measurement in smaller units than milliseconds is not available. Also, note that the Run Time Count includes both the debugger software processing time and the execution time.

However, the E8a emulator supports a method for high precision time measurement using the internal MCU timer. A detailed explanation is provided in the following application note:
E8a Emulator Outline of the Start/Stop Feature and an Example of Its Application for Time Measurement (REJ06J0068-0100)

Suitable Products

E7
E8
E8a