Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Message “Target device driver missing, or connection cancelled.”

Last Updated:04/26/2017

Question:

When I start up the High-performance Embedded Workshop and try to connect to the emulator, I get the following message and the connection fails: “Target device driver missing, or connection cancelled.” What is the cause and workaround for this?

Answer:

If no other error message was generated previous to this message, most likely the emulator software has not been installed.

Please confirm that the software has been installed using the following method.

Start up the High-performance Embedded Workshop and open a workspace. 
If “Device driver not found; connection cancelled” is displayed, click the OK button to close the message box.
From the menu, select [Debug] → [Debug Settings] to open the [Debug Settings] dialog box.
Select <none> from the target drop-down list.
Click the OK button to close the [Debug Settings] box.
Re-open the [Debug Settings] dialog box and confirm that the emulator is included in the target drop-down list.
If it is not displayed in the list, this indicates that the target emulator software has not been installed. Install the software and try the emulator connection again.
 

 

Suitable Products
E1 [R0E000010KCE00]
E20 [R0E000200KCT00]
E10A-USB
E8a
E10T-USB
E8
E100
E200F
E6000H
E6000