Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How to select [Debug] -> [Connect] when an icon didn't appear?

Latest Updated:05/07/2008

Question:

The "Connect" icon does not appear on the screen and I can't select [Debug] -> [Connect].

Answer:

Select [Debug] -> [Debug settings] in the High-performance Embedded Workshop menu, and then open the [Debug settings] dialog and confirm that the target setting is the E10A-USB SYSTEM that corresponds to the MCU you are using.
Suitable Products
E10A-USB