Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

E10A and E10A-USB emulator compatible with SH7147 and SH7142

Last Updated:09/27/2017

Question:

Is there an E10A emulator or E10A-USB emulator that supports SH7147 and SH7142?

Answer:

The E10A-USB emulator unit cannot be used as is because SH7147 and SH7142 MCUs do not embed debugging functions. However, the SH7417 Debug MCU Board (sold separately) can be used with the E10A-USB emulator to enable debugging. For more information, click here.
Suitable Products
E10A-USB
E10A
  • Este artigo foi útil?