Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Can the CS+ display the members of a structure in real-time?

Latest Updated:10/27/2014

Question:

Can the CS+ display the members of a structure in real-time?

Answer:

CS+ is not capable of displaying the members of a structure in real-time.
CS+ displays "?" in such cases because the difference between the time the address indicated by a pointer is acquired and the state of the pointer is generated may lead to the display of an incorrect value (reference to the state of a pointer may lead to display of the value of another pointer).
Suitable Products
CS+ (formerly CubeSuite+)
E1 [R0E000010KCE00]