Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Can H8S/Tiny Series MCU be debugged using E10AUSB Emulator?

Latest Updated:05/07/2008

Question:

Can H8S/Tiny Series MCUs be debugged using the E10A-USB Emulator?

Answer:

No, the E10A-USB Emulator cannot be used for H8S/Tiny Series MCUs.
You will need to use the E8a Emulator.

However, the H8S/Tiny Series MCU debug interface is compatible with the H8/300H Tiny Series.

Suitable Products
E10A-USB