Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Using Boolean algebra (CC-RL)

Last Updated:06/14/2017

Question:

How can I use Boolean algebra while using RL78 compiler CC-RL?

bool AAAA(void)

Answer:

CC-RL supports _Bool-type. See the user’s manual for details.

CC-RL Compiler User’s Manual
4.1.4 C99 language function
(3) _Bool type

 

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family