Pular para o conteúdo principal
Renesas Brasil - Knowledgebase

The state of registration of the license key when updating a revision (CC-RL)

Last Updated:04/17/2017


I am using the RL78 compiler. The evaluation edition which has been released on the Web is a newer version than the compiler that I am using. Will my registered license key be lost if I install the evaluation edition?


You can use the registered license key as it is.
Revising both types of C Compiler for the RL78 Family (listed below) is possible. However, since only the revision (not the version) is updated, you can still use the registered license key as it is.
・CA78K0R compiler
・CC-RL compiler
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family