Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Selecting the Language for Error Messages_CC-RL

Last Updated:02/21/2018

Question:

I am using RL78 Compiler CC-RL.
Is it possible to refer the compilation error messages displayed in Japanese in English?
If not, can I get the list of those messages in English?

Answer:

The language for messages cannot be selected.
If you use the Japanese edition of Windows, messages are displayed in Japanese; in the other editions, messages are displayed in English.
For a message list in English, refer to the English edition of the user's manual.
CC-RL Compiler User's Manual
 10. MESSAGE
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • Este artigo foi útil?