Professional Edition License Operates as Evaluation Edition_Floating License
Last Updated:12/13/2017
Question:
I am building an environment with a floating license. I have registered a license key of the professional edition in a server PC. When building in a client PC, I get a message which says the license is the evaluation edition. How do I resolve this?
In addition, when I acquire the license in offline mode, the message does not appear during building.
Answer:
For the floating license server administrator software, select the [Offer the upper-level license if lower-level license is empty.] checkbox in [Option].
Suitable Products
C Compiler Package for RH850 Family |
C/C++ Compiler Package for RX Family |
C Compiler Package for RL78 Family |