Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is there any difference in compilers when using a node-locked license and when using a floating license?

Last Updated:05/17/2017

Question:

Is there any difference in compilers using a node-locked license and when using a floating license?

Answer:

No. You can use the same compiler with whichever license you have.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family