Pular para o conteúdo principal
Renesas Brasil - Knowledgebase

E0562320 Error Message: “.const” (CC-RL)

Last Updated:06/14/2017


I am using the RL78 CC-RL compiler. How do I resolve the following error?

“E0562320: Section address overflowed out of range : ".const"”


This error message appears when the .const section has been allocated in an invalid address.
The .const section should be allocated in the mirror area (ROM side).
See the hardware manual for the MCU you are using to check the address area of the mirror area, then allocate the .const section in the mirror area (ROM side).

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • Este artigo foi útil?