Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

C Compiler Package for RL78 and 78K (CA78K0R) with CS+ for CC

Last Updated:02/21/2018

Question:

I was using the C compiler package for RL78 and 78K (CA78K0R) before and am now using CS+ for CC integrated development environment.
Can I use CA78K0R with CS+ for CC by registering the CA78K0R license key?

Answer:

There are currently two types of C compiler for the RL78 family as follows.

  C compiler package for RL78 and 78K families (CA78K0R) (earlier compiler)
  C compiler package for RL78 family (CC-RL) (new compiler, launched in 2015)

The compilers usable with CS+ integrated development environment are as follows:

  CS+ for CA,CX: CA78K0R
  CS+ for CC: CC-RL

CA78K0R cannot be used with CS+ for CC.
In addition, the above compilers are sold with a respective license.
Therefore, you cannot use CC-RL with CS+ for CC by registering the CA78K0R license key.
 

Suitable Products
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 and 78K Families
C compiler for RL78 Family and 78K0R