Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Which value is read when timer counts and counter is read at the same time

Latest Updated:03/03/2010

Question:

When the timer counts (the count source is input) and the counter is read at the same time, which value is read?

Answer:

The value read is the value before the timer counts.
Suitable Products
R8C/1x
R8C/2x
R8C/3x
R8C/Lx
R8C/Mx