Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

When not using WDTOVF# pin, is setting of NC okay in every situation?

Latest Updated:03/11/2008

Question:

When not using the WDTOVF# pin, is a setting of NC appropriate in every situation? (acknowledged as output pin at any given time)

Answer:

Yes. Since the WDTOVF# pin is output-only, set it to NC (Non-Connection) when not in use.
Suitable Products
H8S/2678, 2678R
H8S/2668
H8S/2655
H8S/2649
H8S/2643
H8S/2633
H8S/2615
H8S/2612
H8S/2378, 2378R
H8S/2368
H8S/2398, 2357
H8S/2355
H8S/2350
H8S/2345
H8S/2339
H8S/2329
H8S/2319
H8S/2282, 2280
H8S/2117, 2117R
H8SX/1663
H8SX/1657
H8SX/1653
H8SX/1650, H8SX/1651
H8SX/1648A, H8SX/1648L
H8SX/1638, H8SX/1638L