Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

When does the watchdog stops if PM12 bit in the PM1 register is set to 1?

Latest Updated:02/27/2012

Question:

When the PM12 bit in the PM1 register is set to 1 (reset when watchdog timer underflows) and the watchdog timer underflows, does the watchdog timer stop at this time?

Answer:

The registers associated with the watchdog timer are reset and the watchdog timer count operation stops. However, the watchdog timer automatically restarts when bit 0 of address FFFFFh is set to 0.
Suitable Products
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/5L
M16C/56
M16C/5LD
M16C/56D
M16C/5M
M16C/57