Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

When creating mask file, is setting procedure same as ROM code protect?

Latest Updated:01/09/2009

Question:

(QzROM)  When creating a mask file using the Mask File Conversion Utility (MM), is the setting procedure using "MASK option" for function set ROM data the same as for ROM code protect? [2009/01/09]

Answer:

No, it is different.
The value of the function set ROM data should be decided according to the user's system settings and included in the program (ROM data). (#107246)
Suitable Products
7545
7546
7547
7548
7549