Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What will happen if I overwrite timer count stop to 0 during operation?

Latest Updated:03/01/2005

Question:

(Timer)   What will happen if I overwrite the timer count stop bit to "0" (count start) again during operation? [2005/03/01]

Answer:

There will be no effect. The count will continue unaffected. (#104777)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7545
7546
7547
7548
7549