Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What to set memory mapping configuration box seen at debugger startup

Last Updated:11/14/2017

Question:

What should be set for the memory mapping in the configuration dialog box displayed at debugger startup?

Answer:

This is an item specified when using a memory other than the internal memory of the device (when using an externally connected memory, or when using a ROM/RAM emulation memory in the ICE).
Nothing need be specified when using just the device's internal memory.
Since the device's internal memory is automatically secured, setting memory that is redundant with this memory causes an error.
Suitable Products
78K Family