Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What is the difference between H8SX and H8S?

Latest Updated:03/26/2009

Question:

What is the difference between H8SX and H8S?

Answer:

H8SX has additional bit:FETCHMD in SYSCR(system control register) and input buffer control register to control input buffer ON/OFF switching.
Suitable Products
H8SX/1600
H8SX/1663
H8SX/1657
H8SX/1653
H8SX/1650, H8SX/1651
H8SX/1648A, H8SX/1648L
H8SX/1638, H8SX/1638L
H8SX/1622